AXIS#.HOME.SET
Description
AXIS#.HOME.SET immediately makes the current position the home position. After using AXIS#.HOME.SET the axis command and feedback will match AXIS#.HOME.P.
AXIS#.HOME.SET can be used when the axis enabled or disabled and in torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist, velocity or position op modes (AXIS#.OPMODE ).
If the axis is in motion when AXIS#.HOME.SET is used, the motion will be stopped and the home position set.
Once the home position has been set, the addition move defined by AXIS#.HOME.DIST is not made.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HOME.SET | 0x5008 | 0x1 | UDINT | - | - | wo | False |
| AXIS2.HOME.SET | 0x5108 | 0x1 | UDINT | - | - | wo | False |